MITSUBISHI ELECTRIC Changes for the Better

Poznaj DataNavigateApp

DataNavigateApp to dedykowana aplikacja dla modułu funkcyjnego MELSEC iQ-R C Intelligent Function Module. Łączy w jednym narzędziu analizę pracy maszyn w czasie, analizę zużycia energii, monitorowanie cykli pracy oraz diagnostykę alarmów.

Dzięki DataNavigateApp sterownik staje się gotowym do użycia narzędziem analitycznym typu plug-and-play. Bez programowania i dodatkowych prac inżynierskich zyskujesz dostęp do:

  • analizy wydajności maszyn w czasie rzeczywistym,
  • monitorowania alarmów,
  • wizualizacji zużycia energii,
  • narzędzi wspierających predykcyjne utrzymanie ruchu.

To prosty pierwszy krok w kierunku inteligentniejszych maszyn, wyższego wskaźnika OEE oraz cyfryzacji produkcji.

Wsparcie doskonalenia produkcji dzięki aplikacjom dopasowanym do Twoich potrzeb

Use apps tailored to your needs to visualise and analyse equipment, driving improvements on the production site. Each app turns machine data into practical insights — no coding, no IT projects. Just open your browser, and start improving uptime, energy use, and daily productivity.

Time-Based Operation Analysis App

Visualise equipment operation status and analyse factors contributing to the decline in operation rates. Instantly see where time is lost and compare shifts, recipes, or days to find the best performers.

Energy Analysis App

Visualize equipment power usage and identify wasted power and areas for improvement. Lower energy per part by optimizing run/idle behavior. An easy first step toward energy transparency

Operation Cycle Monitoring App

Monitor operating time of cylinders and other parts. Detect abnormal signs and performance issues early before it becomes downtime. Prevent irregular cycle times that affect quality and plan maintenance based on actual machine behavior.

Alarm Analysis App

Visualize alarm status and detect frequent or high-impact anomalies. Remove “chronic” alarms that operators see every day and improve machine reliability with minimal engineering effort.

Three key features of the DataNavigateApp

  1. Simple setup: Its intuitive design makes the app easy for anyone to install and use -no programming experience required
  2. Remote monitoring: Monitor your equipment directly from any computer or tablet using a standard web browser -no dedicated HMI devices required.
  3. Easy data collection: Instantly visualise data from the CPU module, with full support for existing equipment through standard CPU communication functions.

The way to set it up

DataNavigateApp Setup

To set everything up simply install DataNavigateApp on a SD memory card and insert it into the C intelligent function module to start using the application. Equipped with a variety of features, DataNavigateApp supports the visualisation and analysis of the production site, helping you take the first step toward IoT and digital transformation in your factory. Web‑based monitoring enables a more flexible work environment by allowing remote access from any browser.

Steps to activate the license

A license agreement will be provided by the distributor
Enter the product ID and serial number of the C intelligent function module as stated in the license agreement. After completing the application, the license key file will be sent by email.
Download DataNavigateApp from the FA Global website
Install DataNavigateApp on an SD memory card

FAQ

How can I easily connect an energy measuring module using the Energy Analysis App?

How can I easily connect an energy measuring module using the Energy Analysis App?

By using the Energy Package, you can collect energy data from equipment without any programming. The Energy Package is a free energy data collection package that includes a setup tool and a sample project to help you build a production equipment measuring system.

Sample project (for iQ-R CC-Link IEF Basic)

  • Energy data collection program

Setup tool

  • Easy energy measurement setup with drop-down selection

    How to use it

    1. Write the sample project to MELSEC iQ-R 
    2. Set the energy measurement parameters (select from drop-down list) 
    3. Link the device to the Energy Analysis App to complete the setup